This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

PCA9306: Logic level for EN pin

Guru 12900 points

Part Number: PCA9306

I didn't find EN input threshold for High and Low level on the datasheet. 

I guess that EN High: 2.0V_min and Low: 0.8V_max, is it correct?

If not correct, please let me know correct Enable input High/Low level.

Best regards,

Satoshi

  • Hi Satoshi-san,

    EN is actually not a logic input. It is an analog input used by the device to generate a gate bias for the internal switches. We recommend tying it to VREF2 and pulling it high via a 200-kOhm current-limiting resistor in order to operate with the device active. The EN pin could be pulled to 600 mV or lower to disable the device (make it high impedance).

    Max

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.