hi all,
a customer of mine started using the TCA9800 that was placed before an isolator on an I2C bus; but when he tried out the configuration an oscillation appeared on the SDA line. He figured out that the isolator output voltage is somewhere 600mV and the TCA9800 didn't really like it, as it started to pull up and down the voltage on SDA line above 100mV.
To avoid this problem he looked search for anoter isolator with low output voltage, but unfortunately he didn’t find one.
After this the solution became a simple voltage level translator in between, and it works perfectly.
I think the problem with TCA9800 is the active current source which is a good feature but in this configuration it is not necessary for us and unfortunately it causes problems.
may you help me undertanding the root cause of the problem?
thanks a lot in advance
KR
Vincenzo