Dear fellows,
I am looking for Industrial RS-232 to TS-422/485 Converter with the following parameters:
Operating Temeperature : -20 to +50C.
Storage temperature : -10 to +50C/
Operating Humidity : Up to 97% condensing.
I will be glad to get information about relevant product.
B.R
Hezi
Hello,
I'm also in search of a good RS232-RS485 (2 and 4 wired switchable) converter with isolated interfaces but I also need this converter to be able to detect baudrate automatically. Can you suggest me a reliable industrial design solution?
unfortunately we do not have a solution for this full-featured converter. I suggest searching the Internet.
You will probably find entire converter modules providing this functionality.
Regards, Thomas