This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

SN65HVD72: RS485 with AutoDirection

Part Number: SN65HVD72

Dear Sir 

May I know which TI solution can support RS485 AutoDirection ,just like MAX13487E/MAX13488E

Thanks

  • Hi Kai,

    TI does not have a transceiver which is directly compatible, although similar behavior can be achieved with a standard RS-485 transceiver by implementing failsafe termination (A pin pulled high, B pin pulled low), tying the D input low, and then controlled DE to be high to send "zero" bits and low to send "one" bits.

    Another way of implementing automatic direction control of an RS-485 transceiver is to use a monostable multivibrator to enable the transceiver whenever a data frame causes the D input to toggle. Here is a reference design implementing this approach:

    www.ti.com/.../tida-01090

    This circuit has the advantage of maintaining RS-485 compliance by actively driving both the "one" and "zero" levels.

    I hope this helps - please let me know if you have any other questions.

    Regards,
    Max

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.