• TI thinks resolved

ISO5452: Clamp pin internally connects to GND2 or VEE2?

Part Number: ISO5452

Hi Team,

Customer wants to verify with us "Clamp pin:" internally connects to GND2 or VEE2?

Correct me if I am wrong. My understanding is VEE2.

If VEE2 is supply by -5V. Clamp pin should be triggered when incoming voltage reaches -5V + 2.1V = -2.9V typ.

Thanks for verifying.

Andrew