This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TLK10232: TLK10232

Part Number: TLK10232

Hi,

  if I want to use 10.3125G at TLK10232, could I use general purpose mode?

 if it must run at 10G-KR, does it must use clause 45 mode? 

Thanks

  • Hello Cannie,

    You can use general purpose mode at 10Gbps. Please see section 1.3 of the datasheet.

    Regards,
    Yaser
  • In reply to Yaser Ibrahim:

    Hi,

      I need 10.3125G. Also, it need 64B66B coding. in general mode, does it OK?

    Br,

  • In reply to cannie chang:

    Hello,

    The max line rate in general purpose mode is 9.8304 Gbps (see table 5.2). Also, 64B/66B encoding cannot be used in general-purpose mode.

    Regards,
    Yaser

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.