Dear Specialists
My customer is evaluating the ISO724x.
The device was latched up, when the noise was impressed.
What reason is considered?
Could you please see the following.
Conditions
ISO7241 was installed with FR4 4layers and 6 layers, Vcc1=3.3V,Vcc2=5.2V
When radiation noise 0.5kV was impressed from 1cm of distance, the output of secondery side was halted.
At the same time, Icc2 was increased from 16mA(normaloperation) to 680mA.
This phenomenon was happened at ISO7240 and ISO7241.
Question
Why this phenomenon is happened?
The customer is considering this may be latch up.
What measures are considered?
Best regards,