Good day
I am interested in using the ISO7241 in an isolated application.Can you please confirm how much current can be sourced from the Vcc2 pin for powering some external components?
Thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kevin,
ISO7241 is a 4 channel digital isolator. Both VCC1 and VCC2 have to be provided externally. Are you interested to know how much current the Vcc2 pin draws? If yes, it will need a maximum of 28mA during 25Mbps of operation.
Regards,
Sarangan
Hi Kevin,
If you are looking to create an isolated power supply for the second side of the IC, I would recommend looking into the SN6501 or the TPS55010.
Please let us know if you have any questions.
John
Hello Kevin,
The ISO7241 is a digital isolator requiring two supply voltage, on the primary side it is Vcc1, on the secondary side it is Vcc2. Both supply terminals are sinking current.
Future isolators that provide an internal isolated power supply from the primary to the secondary side are on our roadmap but not available yet.
To provide power across the isolation barrier we have a transformer driver IC (SN6501) that can provide power to both supply terminal plus ample current drive capability for data converters and amplifier components.
At the end of the attached data sheet you find plenty circuit examples for isolated data transmission (RS-232, RS-485, CAN, I2C, etc.), isolated data conversion (ADC and DACs), and isolated high-voltage digital inputs.
Kind regards,
Thomas.