Hi,
I need to conned several devices which grounds have a DC voltage difference that can vary between 0 to 100 volts with the master's ground. I think on using a ISO1540 per device.
Is it ok to have this voltage difference between GND1 and GND2? from the datasheed I understand that as long as this difference of voltage between GND1 and GND2 is less than 566 Volts (Viorm) the device will operate correctly.
I need to confirm this. Because there are some discussions on how to understand this insulation parameter.
Best Regards,
Ezequiel