Hello all.
About SN75HVD1176's question.
There is following description in p2 of datasheet.
-------------------------------------------------------------------------------------------------------
(ABSOLUTE MAXIMUM RATINGS)
- Vcc(Voltage input at any D, DE or RE terminal) : –0.5 to 7 (V)
(RECOMMENDED OPERATING CONDITIONS)
- VIH(D, DE or RE) : 2 to Vcc (V)
-------------------------------------------------------------------------------------------------------
Our customer would like to supply 5V at D(#4) pin,when it didn't supply power to Vcc.
Is it no problem when is the above condition?
If it's problem,please tell me any advice.
Best regards,