Hello all!
I have a customer who is interested in isolated USB (Full Speed 12Mbps).
I'm suggesting the miniature 1W 5V DCP010505BP isolated DC/DC for USB power.
I wonder if there is possible to use our ISO-family for the USB two wire communication half duplex? Any appnote showing how to do it, or?
ADI do have the ADuM4160 family not sure if my customer knows about it and i would like to try to get this socket anyway.
The isolation requiremet is low and the only reason for isolation is to isolate the senitive board from the PC ground hum.
cheers