The datasheet describe VCC1<VCC2 cases only. In there any problem VCC1>VCC2 case?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The datasheet describe VCC1<VCC2 cases only. In there any problem VCC1>VCC2 case?
Hi Keiichi,
VCC1>VCC2 case is not a problem. The ISO1540/41 datasheet describes two sets of data, one for VCC1 and VCC2 both being in the 3.0V to 3.6V range, and the other for VCC1 and VCC2 both being in the 4.5V to 5.5V range. However, the device can be used with VCC1 and VCC2 independently in either range.
Rgds,
Anant