The ISO1050 datasheet describes a bus-fault protection of -27V to 40V. Are these CAN_H and CAN_L over-voltage protection clamping voltage? I would like to determine what would happen if CAN_H or CAN_L is shorted to say 30V, will the VCC2 gets pulled to 30V as well. The equivalent I/O schematics diagram suggests that VCC2 is protected (CAN_H line) with a diode but what about the input circuit?