My requirement is to power a rs422 interface from an isolated 5Vdc power supply,
I am using a 28335 micro controller.
I plan on using a iso35, with one power supply connected to the 5Vdc isolated supply, and the other iso35 supply to a 3.3 Vdc supply to feed my microcontroller.
Vcc max for iso35 is 6Vdc, but the part calls out 3.3Vdc (normal operating conditions).
Can this part be used in this manner, isolation and voltage converter,lack of a better description.