This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About skew time of ISO7640FM

Guru 19485 points

Are tsk(o) and tsk(pp) spec condition of 25℃?

Or is it spec condition of -40℃~125℃?

When having spec information on skew time by the temperature range, please let me know.

Especially, I'd like to know a spec of -20℃~60℃.

Best regards,

Satoshi