Hello ,
In want to interface Incremental encoder senosor output to Microcontroller which is 10Meters away from the sensor.
Specifications:
Sensor Output : Square wave 0V to 5V , 100KHz frequency.
Controller: F28M35H52C, EQEP module interface.
As per my understanding, the avaialable options are:
1. Convert sensor output to differential ended signals using RS422/LVDS etc....
2. Convert sensor output to differential ended signals using OP Amps etc....
Is my approach correct,..?
Kinldy suggest the best method(s).
Thanks in advance.
Regards,
Govind.