Hi Team,
My customer is looking for the RS-485 transceiver.
The requirement of the device is the following.
-------------------------
- supply volatge: 5V
- No. of TX/Rx: 2/2(ideal) or 1/1
- Duplex: full
- IEC61000-4-2 Contact Discharge: 8kV
- IEC61000-4-4 Fast Transient Burst: 1kV
-------------------------
Is there any TI device that meets this requirement?
I couldn't find the device on TI web...
Best Regards,
Yaita / Japan disty