This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD01 / about IBIS model

Other Parts Discussed in Thread: SN65HVD01

Hi,

Please let me know whether the following points for SN65HVD01 IBIS model are correct.

Regarding the definition of [Ramp], AB_hs's [Ramp] are smaller than AB_ls's.  Is this correct ?

※AB_hs   high speed AB buffer operation

[Ramp]

R_load = 27

dV/dt_r     1.31081/5.41776e-09(typ)   0.971551/1.10314e-08(min)    1.57638/3.70288e-09(max)

dV/dt_f     1.18121/5.49901e-09(typ)   0.973025/9.69578e-09(min)    1.36243/3.64603e-09(max)


※AB_ls   low speed AB buffer operation

[Ramp]

R_load = 27

dV/dt_r     1.31059/4.98207e-09(typ)   0.971543/1.04064e-08(min)    1.57601/3.41618e-09(max)

dV/dt_f     1.09683/5.29281e-09(typ)   0.854744/9.37254e-09(min)    1.32391/3.5372e-09(max) 

Best Regards,

Kato