This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CAN Datasheet SN65HVD231

Other Parts Discussed in Thread: SN65HVD231

I was perusing the datasheet for SN65HVD231 CAN transceiver (SLOS346L March 2001 revised January 2015) and found a number of errors:

1. In section 13.1 of layout it says "An example placement of the Transient Voltage Suppression (TVS) device indicated as D1 (either bi-directional diode or varistor solution) and bus filter capacitors C8 and C9 are shown in ."   Shown in WHERE?

2: The chart which indicates slew rate has the Y axis labeled as "Outout"  and the X axis as "resistance in kW"

Can you comment on these errors?

Jason Haedt