SN65LVDS100 Single-end LVPECL Input interface
Hi
In the data sheet page26 Figure47 of SN65LVDS100 There are circuit example of Single-End.
+ Side input of SN65LVDS100 is tied to GND with a 50Ω.
I think the input signal GND to center amplitude in this connection.
50Ω termination resistor is I believe is correct to connect to VBB.
About my ideas, please comment.
Best regards