Hello,
Can we connect the GND of ISO7640 and ISO7140 to negative voltage ?
For example, can we use these device at the following supply conditions?
Vcc1=3.3V, GND1=0V
Vcc2=2.5V, GND2= - 2.5V
Best Regards,
Ryuji Asaka
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.