Hi,
Is TI having RS485 line driver ICs with auto direction control .If so please suggest the part number
Regards
Eby
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Eby,
TI currently does not offer any RS-485 transceivers with auto direction control.
This feature can be implemented externally though through the use of a timing control one-shot circuit or a timing control circuit using an inverting buffer. In both of these applications the transceiver driver enable pin is controlled by the external timing circuits enabling auto direction control. A colleague of mine wrote a great application note on this topic and you can read it here.
Please let me know if you have any questions about the circuit implementation and I will be glad to help!
Hi Eby,
We did a reference design for a bus that shares an RS-485 transceiver and a RS-232 transceiver, below is a PDF of the schematic. We designed the board to support two full duplex RS-485 transceivers and two full duplex two channel RS-232 transceivers. Each device is enable via a jumper on the board.
After you review this I can answer any questions you have and I can also provide you with the rest of the required board file (i.e. BOM, Gerbers, and Layout). I also have a board in the lab that I can send you for further evaluation.In return could you please tell me the company that you are with and the end application you intend to use this in? We like to track this information to see what customers are using which devices in what applications. This helps us better support you in the long run. We can move the conversation off line if need be. My email address is mpeffers@ti.com.
Hi Eby,
The RS-232/RS-485 implementation isn’t really dependent on the processor platform used, the schematic I provided can still serve as a good reference. The single-ended transmit and receive connections to the existing RS-232 transceiver can be shared by the RS-485 transceiver as long as the enable pins are properly handled so that only one type of transceiver is active at a given time. The only other thing maybe to point out is that RS-232 has a pretty large signal swing, so the RS-485 transceiver needs to have a large enough fault tolerance/standoff voltage rating to not be damaged by the 232 transceiver.
I hope this answers your questions?