Hi all
Would you mind if we ask DS26LV32ATMX and DS26LV31TMX/NOPB?
<Question1>
These datasheets show min and max value of tPLHD and tPHLD.
So, do you have these typ value as the reference?
Because there is the large difference between min value and max value.
<Question2>
The datasheet shows that tSK(skew tpHLD-tpLHD) is max 6.0 nS.
So, does it include following conditions as example;
-tPLHD : 39ns
-tPHLD : 33ns
Kind regards,
Hirotaka Matsumoto