Hello,
We consider applying a ti digital isolator like ISO742x.
We apply a 100kHz PWM signal with wide varying duty range. T=10us, ton 50ns ... 9950ns.
The functional block diagrams shows separate signal paths for f=DC...100kHz and for , f>100kHz.
When duration between two consecutive transient exceeds a certain time limit the multiplexers switches to the LF signal path.
Question1: What is this time limit? I guess ~5us but is not not listed in the datasheet.
Question1: Is operation stable when the applied signal is around this 100kHz? I am concerned the multiplexer might toggle with f=100kHz, duty=50%.
Question 3: Do the listed switching characteristics still apply for signals f<100kHz. For instance is t_prop still low when f=90kHz?
Kind Regards,
Maikel Sturkenboom
High Voltage Engineering
the Netherlands