Question: Using a SN6505B together with transformer WE 750315371 is applicable for currents up to 1A?
SN6505 Datasheet Table 3 Shows "Application" 5 V → 5 V ,100mA, but related Figure 3 and 4 do Show current up to 925mA.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Question: Using a SN6505B together with transformer WE 750315371 is applicable for currents up to 1A?
SN6505 Datasheet Table 3 Shows "Application" 5 V → 5 V ,100mA, but related Figure 3 and 4 do Show current up to 925mA.
Hi Gerhard,
You are right. The table has a typo. SN6505B is suitable for 1A operation. The figures are correct.
We'll correct the datasheet. Thanks for pointing this out.
Rgds,
Anant