Hello Community!
I have an urgent question on the ULN2803A:
I would like to use the ULN2803A as a relay driver. My question is: can I connect to 1 channel 2 relays in parallel?
The coil current of my relays is 84mA, so two relays would be at 168mA. The ULN2803A allows 20-300mA per channel, so I assume this would be ok, correct?
But can I connect two in parallel as long as I don't exceed the 300mA per channel?
Thank you very much for your help!
David