Hi e2e,
Our customer is having problems with the TCA8418, it is giving false touches when the membrane is touched and the snap domes are not depressed and it is locking up if too many keys are pressed. Can you pleased assist, please see full description from customer below.
The two problems are as follows:
1.) We are getting false key presses when rubbing the keypad membrane while our processor board is plugged into a power source. Our keypad normally runs on a battery and we do not see false key presses when Keypad is not plugged in.
2.) We are experiencing a stuck key every so often. Normally this occurs when multiple buttons are pressed at the same time. We believe this to be an issue with the resistance of the pull-up on the interrupt and reset pins.