Hello,
A customer is using a quad RS485 driver (SN65LBC172A) and he wants to know if the input pins can tolerate a high input signal when the device is powered down. The datasheet says the maximum voltage the input pins can tolerate is Vcc + 0.5 V, but I am assuming this refers to Vcc when the device is turned on.
We just want to make sure that the device will not be damaged when the input signal is high and Vcc = 0.
Thanks,
Daniel