I have several PCBA's which do not have a heartbeat. I'm a test engineer so I'm neither the SW or HW designer. The CANH and CANL lines have 2.4Vdc. We use two 120 Ohm terminating resistors at each end with the inside leads tide to ground via a cap. We use a TMS470R1B512PGET microP to our transceiver SN65HVD1050. Resistances look fine, voltages (at least on a DMM) look fine. Not sure where else to look. Can you recommend some other avenues which I might be able to travel?