Hi all,
Our customers are considering a change from competitors products to ULN2803A.
They have question.
When the input port pulled-up to 3.3V by 3.3kohm resistor,
How much the Vce(sat) at Ic=50mA, 80mA and 100mA?
Regards,
Nagai
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
Our customers are considering a change from competitors products to ULN2803A.
They have question.
When the input port pulled-up to 3.3V by 3.3kohm resistor,
How much the Vce(sat) at Ic=50mA, 80mA and 100mA?
Regards,
Nagai
Hello Nagai-san,
Here is what I can answer:
- When If=500mA, is there a limit to the current pulse width of this device?
At 25C, the device can manage 500mA continuous current through the diode.
- When If=350mA, can this diode flow the continuous current?
Yes, at 25C, this current can flow continuously
- How much the maximum reverse-recovery-time (Trr)?
I was able to measure the reverse recovery time of the diode on the bench. The recovery time will depend on the current flow in the ON state as well as the voltage applied to reverse bias.
I found that with 250mA forward current and -0.4V reverse bias, the reverse recovery time is around 250ns. Note this was taken for a single unit at room temperature and is not a guarantee of the device specification.
Best,
Michael