This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD230Q-Q1: static connection with other device

Dear all,

Could you teach me following two topics?

1, Can this device communicate with TJA1051?

2, Can this device serve as a substitute for TJA1051?

Best regards,

  • Hi Takao,

    1. Yes the SN65HVD230Q1 will communicate with the TJA1051.

    2. The SN65HVD230Q1 can serve as a substitute for the TJA1051 although it is a 3.3V device. We have a pin for pin compatible TCAN1051Q1 that would be a better option unless 3.3V is the way you want to move.

    Please let me know if you have any more questions.