Other Parts Discussed in Thread: , TPL7407L
Hello,
I have two questions about ULN2003A.
I attach a file.
Regards,
Dice-K
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Ronald and Michael,
Thank you for your replies.
I have a question about your answers.
"The ULN2003AI has a 30uA minimum for off current (at 105C) , where 'off' means 500uA of output current flow."
"The key here is to look at the specification for Ioff.
Ioff minimum specification is 30uA, so it should be designed to meet this minimum specification."
Do these answers adapt to ULN2003APWR?
ULN2003APWR (Ta:-20C~70C)
ULN2003AIPWR (Ta:-40C~105C)
Best regards,
Dice-K
Hello Michael,
Thank you for your reply.
Though the temperature range of ULN2003AIPWR is different from ULN2003APWR, I understand that the specification of Ii(off) is same.
ULN2003APWR (Ta:-20C~70C) Ii(off)=30uA
ULN2003AIPWR (Ta:-40C~105C) Ii(off)=30uA
If my understanding is incorrect, please give me a reply.
Best regards,
Dice-K
Hello Michael,
Thank you for your reply.
It is the matter of Ii(off)=30uA.
Is this an electric current that includes the electric current of the resistance and the base electric current to a transistor of the internal circuit?
In the case of the circuit of the customer, when VI=0.7V (series resistance =5.1kohm), an electric current of 39uA flows only by internal resistance.
How much is the base electric current?
In the data-sheet, Ii(max)=1.35mA at Vi=3.85V.
Because the internal resistance consumes about 0.3mA, is this base electric current 1.05mA?
Best regards,
Dice-K
Hello Michael,
Thank you for your reply.
Please teach me a base current with Fig8 and fig6.
For example, when output current is 200mA, Ii is 350uA.
When Ii is 350uA, Vi is 2.5V.
Because internal resistance is 12.9kohm, the base current is 350uA-(2.5V/12.9kohm)=156.2uA.
Is this calculation correct?
Best regards,
Dice-K
Hi Dice-K,
Ultimately, the important information is the input current vs. the output current. This will determine the amount of input current needed to drive a specific load, and the amount of current going into the base of the transistor will be a part of that.
If you did need some additional information, we have some data (below) which plots the DC current transfer ratio (beta) vs. IOUT. As evidenced by the graph, the base current is going to depend on the output current.
Thanks,
Alek Kaknevicius
Hello Alek,
Thank you for your reply.
My customer has a question about the following sentence.
"This will determine the amount of input current needed to drive a specific load,
and the amount of current going into the base of the transistor will be a part of that."
For example, by the given graph, when the output current is 10mA, hfe is 80 at Ta=-40C.
Therefore the input current 'Ii' is 10mA/80=0.125mA.
I think that this 'Ii' is 'input current needed to drive a specific load'.
Does this 'Ii' mean 'internal resistance current + base current + α'?
Doesn't this 'Ii' mean 'internal resistance current + base current'?
Best regards,
Dice-K
Hi Dice-K,
I agree with your definition, Ii is the 'input current needed to drive a specific load.' This is the total current flowing into one of the input pins for a specific output current.
Why does the customer need to know how much of that leakage is internal resistance current and how much of it is base current? Isn't the only concern the amount of input current needed for a specific output current?
Thanks,
Alek Kaknevicius
Hi Dice-K,
This leakage is measured with both the COM pin and output left floating, so the input leakage seen here is only between the input and ground. With a load, this current could increase.
Thanks,
Alek Kaknevicius
Hello Alek,
Thank you for your reply.
My understanding is as follows.
When 'Vi is 3.85V' and 'the output load is zero' and 'COM pin is floating', the maximum input current is 1.35mA.
ULN2003A does not need 1.35mA input to make output.
(Figure-8 shows this.
For example, when Input current is 250uA, Output current is 100mA.)
Is my understanding correct?
Best regards,
Dice-K
Hi Andrew,
Yes, it is possible to have 16V on the output pins (xC) and 5V on the control pins (xB). Could you please elaborate on your question about current on each leg? Figures 4 and 5 in the datasheet do a very good job of explaining the amount of current which can be applied on each channel if a certain number of channels are active.
Thanks,
Alek Kaknevicius
Hi Andrew,
Yes, the inputs are pulled down by the internal resistors to ground.
As for the 2A requirement, we do not have any devices which can do this without putting multiple channels or devices in parallel. The TPL7407L is an option which would allow for more current/channel, but the amount of current per channel is dependent on the duty cycle for your load. Assuming a worst case scenario of 100%, you would need two devices and about 12 channels in parallel.
Thanks,
Alek Kaknevicius