This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN751178: VOH/VOL of SN751178

Part Number: SN751178

Dear Sirs,

My customer asked us about VOH/VOL of SN751178.

At the output of the Receiver circuit,
What is the certified value of Voh / Vol at current (3 mA, 5 mA, 10 mA, 16 mA, 20 mA)?

(Because、when they use this device, there is a possibility that the current may flow by 5 to 20 mA.)

Best Regards,

Y.Hasebe