Other Parts Discussed in Thread: AM26C31
Hello Team,
Our customer uses AM26C32 receiver together with AM26C31 in a repeater system.
Occasionally they face the problem that another equipment in the system can inject up to +/-15V into the repeater. This is exceeding the absolute max ratings of the device.
The question is:-
Apart from the note (1) on under section 6.1 which writes the device may be damaged, can we predict the failure mode during this condition?
Will the high voltage at the input be propagated to the output of the repeater?
Best regards,
Mizanur Chowdhury
Central Application Engineer & Mass Market FAE
North East Europe (Czech, Latvia, Lithuania, Poland & Slovakia)
TEXAS INSTRUMENTS