ULN2003A absolute maximum rating of TA is -20 degC to 70 degC. And Recommended Operating condition Tj is -40 degC to 125 degC.
Should we use ULN2003A within TA -20 degC to 70 degC even if device power consumption is low and Tj is not over 125 degC?
Using condition is the following,
1ch to 4ch: 7mA at each ch
6ch: 120mA
5ch, 7ch: not used
Best Regards,
Kohei Sasaki