This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1051HGV-Q1: TCAN1051 Shield Mode

Part Number: TCAN1051HGV-Q1
Other Parts Discussed in Thread: TCAN1051

Hi , 

I amd wondering if our device TCAN1051 support also the shield mode. It is not really describe in the datasheet

"The proposed CAN FD Shield transceiver provides three operation modes. In normal mode, it behaves as specified in ISO 11898-2. The RXD signal represents the bus lines and the TXD signal controls the transmission caused by the connected CAN controller. In stand-by/sleep mode the RXD signal is high (recessive) as long as no wake-up event has been detected. Upon wake-up, the stand-by state is entered. The RXD signal is switched to low (dominant) until the transceiver leaves the stand-by state by request of the attached micro-controller. In shield mode, the RXD signal is low during the data-phase of any CAN FD message. The TXD input is disabled; this means the transmitter is not active. Shield mode cannot be requested by the micro-controller. It is entered automatically from normal mode, while a CAN FD message is on the bus."

Thanks and regards, 

Mohamed