Hello,
Our customer use the AM26LS31,using with transceiver IC (SN75176).
The customer connect the AM26LS31 and the SN75176.
When power on, the driver of the SN75176 output high level for a while.
So, the low state output terminal of the AM26LS31 is damaged.
The DS26LS31 has short circuit protection.
Can the DS26LS31 avoid a damage as described above?
I thought the protection effective for only output short (Y and Z)......
Best Regards,
Naoki Aoyama