Dear Sirs,
My customer asked us about StanbyMode in parallel connection of TCAN1042V-Q1.
They are using CAN BUS in parallel connection
One is a BUS using TCAN 1042 V-Q 1, and the other is using another device
So the condition is TCAN 1042V-Q1 as StanbyMode and the other Bus is communication status.
In that case, is there any impact on the other Bus?
When I asked the other day, I got an answer that StanbyMode is defined as 0V.
My customers are concerned that the communication side will be affected under the conditions of parallel connection and 2.5 V at Ressesive during communication and 0 V at Stnaby Mode.
Best Regards,
Y.hasebe