Part Number: TP3054
Hello!
Can we replace TP3054 with TLV320AIC1106, while we are using only DAC portion of TP3054 (igrore the ADC portion).?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TP3054
Hello!
Can we replace TP3054 with TLV320AIC1106, while we are using only DAC portion of TP3054 (igrore the ADC portion).?
Hi, Zain,
I think you could use the TLV320AIC1110 to replace the TP3054, but you must consider that the 'AIC1106 is optimized for audio applications. There should be no problem in using only the DAC portion of the 'AIC1106.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer
Thanks Diego!
Actually I am using a ( RM57L843, Flash, CODEC) to play the ".wav" files. These files are stored in "Flash" and I have to play these file with "RM57L843 and CODEC". Also I have to do digital mixing ( to play two files at a time). So can you please suggest me a reference design or application note?