Why does this device allow either D5.6 or D16.2 to complete the IDLE character?
Would the device care if I just picked one of them and called it good?
I understand that D5.6 does not have disparity, whereas D16.2 does.
As an example, I could use K28.5 to control my disparity, and use D5.6, since it would not adjust disparity.
Or, I could use D16.2, and both K28.5 and D16.2 would adjust the disparity...
Would the IC be upset if I only set D16.2 or D5.6 after the K28.5?