Other Parts Discussed in Thread: TCAN1043-Q1, TCAN1043
Hello,
-Caution-
There was no "TCAN1043-Q1" as a device registration candidate in E2E.
Therefore, I registered "TCAN1042 - Q 1" instead.
The question is about "TCAN1043 - Q 1".
------------------------------
Questions about TCAN1043-Q1 power up / power down sequence specification
This device has three power supply inputs: VCC / VIO / VSUP.
Is the procedure for Power on / Power off for each power supply input specified?
As far as I see the datasheet,
I could not found a description specifically.
My customer's products use the following supply voltage.
VSUP = 12 V
VCC = 5 V
VIO = 3.3 V
The customer wants to turn on VCC (5 V) after 20 ms after turning on VIO (3.3 V).
Are there any problems with this sequence?
----------------------------
Best Regrds,Orobianco