This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLK10022: Maximum supporting frequency?

Part Number: TLK10022

Hi,

I would like to check availability of 10.24Gbps(2.56X4ch).

I know it can be supported upto 10Gbps.

I was wondering it is possible to change some parameter setting for 10.24Gbps.

please let me know 10.24Gbps transfering is possible or not.

  • Hi Bruce,

    This is not possible, since the TLK10022 supports up to 10Gbps(max) in the high speed side. Since this device use frequency multipliers for low and high speed SerDes and other internal circuits. The unique way is to use 2 to 1 or 3 to 1 to support this data rate (2.56Gbps).

    Best Regards,
    Luis Omar Moran
    High Speed Interface
    SWAT Team