Good day everyone,
I'm currently looking at the UCC21520 and have 2 questions.
1) This is more of a double check, but in a high-side/low-side configuration, I'll be able to switch both transistors on without the device implementing any automatic protection and shutting it off. It seems so from the datasheet, just want to double check that.
2) Lastly, I won't be using this as switching, more for control. So I'll switch on the low side, then the high-side and low-side and lastly just the high-side. So These will all be switched on for a length period ~10 seconds, Therefore a bootstrap probably won't work. It can also be either for longer or shorter periods. Therefore I'd like to couple a isolated ground to the gate of the high-side mosfet, Have this coupled to an dcdc converter and couple the 12V iso output of that to the VDDA of the high side and the iso ground to the high-side VSSA. Will this work in the sense that the chip will function normally in this use case? Is there an alternate method that I could use if this might not work optimally with this chip.
Thanks in advance for any help