The newer RS-485 devices claim to have built in failsafe circuitry.
So if NO external biasing resistors are used, what is the voltage on the A/B lines.
On the other hand, if the master has say 1K Pull-up/down for bias, and 120 Ohm for Termination, then in a 3V3 system, the idle voltages will only be 187mV apart.
This is less than the 200mV some of the information suggests is the minimum.
So unless the External bias resistors are around 750 Ohm to 820 Ohm, with a 120 Ohm Termination, the Vid is too small for reliable communication?
Then that all goes out the window if the Master has 120 Ohm termination, with 500 Ohm Biasing, and the Slave (receiver) has 120 Ohm Termination
This gives a 187mV idle state for Vid (Va - Vb), which is lower than the recommended 200mV?
I guess the
VIT+ Positive-going input threshold voltage of -65mV
and
VIT– Negative-going input threshold voltage of -200mV is a little unclear.
Any help appreciated