We are using a TI AM26C32MWB (DSCC PN: 5962-9164001QFA) in a design and would like to use this receiver for some +3.3V I/O signals that we have. I’ve found a TI app note that outlines a way to do this (see Section5; Figure2):
http://www.ti.com/lit/an/snla041a/snla041a.pdf
Based on that, I have come up with the a termination scheme using a resistor divider (+5V -> 10k -> 4.32k -> GND) on the negative input (B input) to create a +1.5V reference. The A input is the +3.3V I/O signal and will swing between 0V and +3.3V.
Any concerns with this scheme? Improvements?
Thanks
John