Thanks Max,
One more thing I forgot to mention. We'd like to change the behavior of the fail safe inputs such that an open input on the A terminal will output a '0' (low signal). To do this, we were considering a 10k pull down resistor on the A input (+3.3V I/O signal). However, the spice model of the input structure shows a small voltage differential between the two input circuits (A/B inputs with B input held at +1.5V w/divider). A 1k pull down seems to work better to provide a larger voltage differential.
Thoughts here?
Thanks,
John