This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

1.8V to 5V Interface or Buffer

Is there an interface buffer that can translate from 1.8V level to 5 V level?

Most 5V buffers that I can find require Vih(min) = 3.5V at Vin=5V.

Could this buffer also drive a FET gate?

Thanks,

Roger

2 Replies

  • Roger

    How much current would this FET gate require?

    Regards,
    Ronald Michallick
    Linear Applications

    TI assumes no liability for applications assistance or customer product design. Customer is fully responsible for all design decisions and engineering with regard to its products, including decisions relating to application of TI products. By providing technical information, TI does not intend to offer or provide engineering services or advice concerning Customer's design. If Customer desires engineering services, the Customer should rely on its retained employees and consultants and/or procure engineering services from a licensed professional engineer (LPE).

     

  • In reply to Ron Michallick:

    Estimate about 1nF input cap, 5V swing and about 100kHz.
    So I would estimate about 1mA.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.