Hi,
I am looking into the Scansta 101 datasheet, and got curious about whether it is possible to directly control dot1_SM pins (such as TMS_SM or TCK_SM) via input dot1 pins (like TMS or TDI), which will be connected to the external JTAG header.
Without this kind of "bypass" mode, I think I may need to use an additional MUX logic, or disable the output pins (making them being in a tri-state) of Scansta101 by strobing OE pins high, am I correct?
Regards,
Jin