Part Number: TPIC84000-Q1
Hi team,
The customer is using TPIC84000-Q1. First, the customer needs some code routine. Then I provide the code routine that Darren Rollman provided.
Darren Rollman provided the code routine link is :
Please check the attachment for the code routine. Now the customer refers to the code routine to use the TPIC84000-Q1 device to
communicate with MCU through SPI. The SPI commuincation code is as below. The customer would like to verify if the SPI communication is fine.
Would you support the issue?
The SPI commuincation:
// Wake up Message
MCU Send : {0x90, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
TPIC84000 Send : {0x40, 0x00, 0xC4, 0xC1, 0x15, 0x0D, 0x00, 0xC0};
// Program Configuration
MCU Send : {0x90, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
TPIC84000 Send : {0x20, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
// Load Data
MCU Send : {0x30, 0xAA, 0xAA, 0xAB, 0x8B, 0x32, 0x99, 0x5A};
TPIC84000 Send : {0x20, 0x10, 0x00, 0x31, 0x30, 0x45, 0x43, 0x40};
// Program control and status register
MCU Send : {0x20, 0x02, 0x0E, 0x80, 0x00, 0x00, 0x00, 0x00};
TPIC84000 Send : {0x61, 0x55, 0x55, 0x57, 0x16, 0x65, 0x32, 0xB4};
// Start transmission
MCU Send : {0xD0, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
TPIC84000 Recv : {0x40, 0x04, 0x1D, 0x00, 0x00, 0x00, 0x00, 0x00};
// ReadBack from device to get current measurments
MCU Send : {0xD0, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
TPIC84000 Send : {0xA0, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
// Wake up Message
MCU Send : {0x90, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
TPIC84000 Send : {0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
Best Wishes,
Mickey Zhang
Asia Customer Support Center
Texas Instruments