This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MAX3232
In data sheet of MAX3232 C1,C2,C3,C4 values are 0.1uF when VCC is 3.3V.
When VCC is 3.3V, Can we use 0.33uF of C1,C2,C3 and C4?
We want to directly replace the competitor vevice with MAX3232. but cap values are different.